WDOG is not hitting ISR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WDOG is not hitting ISR

1,067件の閲覧回数
Shruthi_C
Contributor III

HI all,

I configured WDOG of S32K146 microcontroller, in TIMEOUT Mode and timeout duration of 500ms, Its not hitting WDOG ISR, inside that I just turned ON LED but not glowing

Please support

Thank You

0 件の賞賛
返信
1 返信

1,052件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Have a look at WDOG direct reset does not enter the interrupt(S32K144) and Example S32K144 WDOG RCM interrupt


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信