Max baudrate LPUART2 for FS32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max baudrate LPUART2 for FS32K144

Jump to solution
3,679 Views
bryan_hong
Senior Contributor I

How much maximum LPUART2 Baudrate can be set for stable communication on FS32K144 

0 Kudos
Reply
1 Solution
3,668 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @bryan_hong,

The LPUART functional clock can be set up to the BUS_CLK freq, which is 56MHz in HSRUN and 48MHz in RUN.

Baudrate = LPUART functional clock / SBR (min 1) * OSR (min 4)

danielmartynek_0-1692193302149.pngdanielmartynek_0-1692193302149.png

danielmartynek_1-1692193332539.pngdanielmartynek_1-1692193332539.png

danielmartynek_2-1692193392737.pngdanielmartynek_2-1692193392737.png

 

That means the baudrate can be even 14 MHz in HSRUN.

This is rather limited by the AC electrical specification of the IOs and by the electrical characteristics of the bus.

S32K1xx, Datasheet, rev14

5.1 AC electrical characteristics

5.2 General AC specifications

Table 23. AC electrical specifications at 5 V Range for S32K1xx series

 

Regards,

Daniel

 

 

View solution in original post

0 Kudos
Reply
5 Replies
3,660 Views
bryan_hong
Senior Contributor I

thanks Daniel for quick updates.

How to get the 14Mhz ?

48/1*(4+1) = 9.6

 

0 Kudos
Reply
3,627 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Theoretically in HSRUN.

56 MHz / (1 * (3 + 1)) = 14 MHz

 

BR, Daniel

0 Kudos
Reply
3,622 Views
bryan_hong
Senior Contributor I

thanks for update

Not theoretically, can this be enabled stable in practice?

Is there a use case for max baudrate that was actually used?

Bryan

0 Kudos
Reply
3,615 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @bryan_hong,

Why do you need this baudrate? I'm not aware of such a use case.

 

With this configuration, there would be oversampling rates of 4x.

danielmartynek_0-1692263064869.pngdanielmartynek_0-1692263064869.png

The baudrate (14 MHz) would have 71.4ns period.

There are no GPIO-HD (PORTn_PCR[DSE] = 1) LPUART pins, only GPIO (PORTn_PCR[DSE] = 0), refer to S32K144_IO_Signal_Description_Input_Multiplexing.xlsx

At 200pF bus capacitance, the slew rate of the pins can be up to 54.8ns / 5V (Rise time), 59.7ns / 5V (Fall time).

danielmartynek_1-1692263651197.pngdanielmartynek_1-1692263651197.png

As you can see, it depends on the electrical characteristics of the bus.

 

Regards,

Daniel

 

 

 

 

 

0 Kudos
Reply
3,669 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @bryan_hong,

The LPUART functional clock can be set up to the BUS_CLK freq, which is 56MHz in HSRUN and 48MHz in RUN.

Baudrate = LPUART functional clock / SBR (min 1) * OSR (min 4)

danielmartynek_0-1692193302149.pngdanielmartynek_0-1692193302149.png

danielmartynek_1-1692193332539.pngdanielmartynek_1-1692193332539.png

danielmartynek_2-1692193392737.pngdanielmartynek_2-1692193392737.png

 

That means the baudrate can be even 14 MHz in HSRUN.

This is rather limited by the AC electrical specification of the IOs and by the electrical characteristics of the bus.

S32K1xx, Datasheet, rev14

5.1 AC electrical characteristics

5.2 General AC specifications

Table 23. AC electrical specifications at 5 V Range for S32K1xx series

 

Regards,

Daniel

 

 

0 Kudos
Reply