Using one TRGMUX source for multiple target module?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using one TRGMUX source for multiple target module?

跳至解决方案
1,947 次查看
JeorgeB
Contributor III

Is that possible to use one TRGMUX source for multiple target modules in S32K14x? 

e.g., FTM0_INIT_TRIG to (DMA_CH0, ADC0_ADHWT, LPUART0_TRG and LPSPI0_TRG)

 

 

Thanks.

 

0 项奖励
回复
1 解答
1,922 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,923 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

0 项奖励
回复