Using one TRGMUX source for multiple target module?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using one TRGMUX source for multiple target module?

ソリューションへジャンプ
1,921件の閲覧回数
JeorgeB
Contributor III

Is that possible to use one TRGMUX source for multiple target modules in S32K14x? 

e.g., FTM0_INIT_TRIG to (DMA_CH0, ADC0_ADHWT, LPUART0_TRG and LPSPI0_TRG)

 

 

Thanks.

 

0 件の賞賛
返信
1 解決策
1,896件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,897件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

0 件の賞賛
返信