Using SENT as Triggered SENT using Flex IO peripheral

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SENT as Triggered SENT using Flex IO peripheral

1,294件の閲覧回数
AVargh23
Contributor III

Can a FlexIO pin be used as an output to send trigger and then receive SENT frames for S32K344? The example project has it set up for FlexIo Sent Receiver alone. Is it possible to make use of the same to act as an output to send trigger pulses to SENT device  and then change it to input to receive the SENT frames? 

タグ(3)
0 件の賞賛
返信
1 返信

1,269件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is apparently not possible to do it with FlexIO. Pay attention to following thread:
https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-FlexIO-configuration-to-SENT-SAE-J2...

 

0 件の賞賛
返信