Unified Bootloader for S32k116_LIN - Issue after ECU Reset.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unified Bootloader for S32k116_LIN - Issue after ECU Reset.

ソリューションへジャンプ
2,690件の閲覧回数
RGMAL
Contributor II

Hello,

I am working with you Unified Bootloader V2 for S32k116_LIN. Which use the UDS Process with CANalyzer but I have a problem after ECU Reset, When my script finishes the UDS process, it will check if it can jump to APP or not but in this step I have a problem and I only see DEFAULTISR.

what could be the root cause of not jumping to APP?

Thank you and Regards!

0 件の賞賛
返信
1 解決策
2,673件の閲覧回数
nxf10035
NXP Employee
NXP Employee

Hello,

   Please check:

  1. Jump Address correct nor not. The address as following picture
  2. If the address correct, please check the APP can working normally or notnxf10035_0-1635318318684.jpeg

     

    Can you upload the log(Capture by CANalyzer)?

Beset Regards!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,674件の閲覧回数
nxf10035
NXP Employee
NXP Employee

Hello,

   Please check:

  1. Jump Address correct nor not. The address as following picture
  2. If the address correct, please check the APP can working normally or notnxf10035_0-1635318318684.jpeg

     

    Can you upload the log(Capture by CANalyzer)?

Beset Regards!

0 件の賞賛
返信