Unified Bootloader Flow Control Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unified Bootloader Flow Control Issue

1,957件の閲覧回数
pratikkul26
Contributor I

Dear Sir/Ma'am,

PFA Log & functions

I'm working on UDS using unified_bootloader_demo_v2.1. I'm using S32K146 controller.

library porting & integration was successful I was able to test services such as session control, read & write data by identifier. 
but when I tried to execute security access service. following happened
1)security access request  sent using GUI/UI "NXP Open Bus" or "ECU Bus".

2)First frame received from the hardware.

then UI/GUI didn't send the Flow control frame.

also I would like to understand how to use can_tp.c functions for receiving & transmitting first frame, flow control frame, consecutive frame etc. does TP maintains the status if transmitted data is more than 8 bytes? 

Regards,

Pratik

0 件の賞賛
返信
0 返答(返信)