Two contradictions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Two contradictions

1,012 次查看
814420552
Contributor III

hello,
The following description conflicts. Which one is right

   pastedImage_1.pngpastedImage_2.png

0 项奖励
回复
1 回复

953 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui,

Both are correct.

"5.2.1.1" is mainly to explain trigger mass erase by debugger. The mass erase similar to Erase All Blocks, but there are a little difference.
A mass erase via the debugger is allowed even when some memory locations are protected.

"36.5.11.11" The Erase All Blocks command (Flash command) aborts if any flash or FlexRAM region is protected.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复