Two contradictions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two contradictions

1,030件の閲覧回数
814420552
Contributor III

hello,
The following description conflicts. Which one is right

   pastedImage_1.pngpastedImage_2.png

0 件の賞賛
返信
1 返信

971件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui,

Both are correct.

"5.2.1.1" is mainly to explain trigger mass erase by debugger. The mass erase similar to Erase All Blocks, but there are a little difference.
A mass erase via the debugger is allowed even when some memory locations are protected.

"36.5.11.11" The Erase All Blocks command (Flash command) aborts if any flash or FlexRAM region is protected.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信