Toolchain Version Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toolchain Version Problem

1,354件の閲覧回数
mayank_x30
Contributor I

hi community i installed s32design studio after importing a exmple iam getting following red cross on project what it might be the issue and how can i solve this issue please observe below marked ones it showing error as Description : Current version of the toolchain is no longer supported. It is necessary to perform project migration to a later version.ErrorErrorInstallation DetailsInstallation Details

タグ(3)
0 件の賞賛
返信
1 返信

1,330件の閲覧回数
IsaulO
NXP Employee
NXP Employee

Hi @mayank_x30 ,

Based on the currently available information, it is not recommended to install S32K1xx SDK 4.0.x in S32DS 3.5, as we have no plans to integrate S32SDK S32K1XX 4.0.x on S32DS 3.5 or above version.
Instead, we recommend installing S32K1 RTD 2.0.x on S32DS 3.5., either online with S32DS Extensions & Updates or offline, HOWTO:offline install S32K1 RTD 2.0.0 in S32DS v3.5.

You can find this RTD version in S32K1 page >> Design Resources >> Software >>
Real-Time Drivers for S32K1 >> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M >> S32K1_S32M24x Real-Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0


BR,
IsaulO.

0 件の賞賛
返信