Time difference LPIT channels immediately after enabling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Time difference LPIT channels immediately after enabling

ソリューションへジャンプ
2,963件の閲覧回数
Joey_van_Hummel
Contributor IV

Hi all,

 

I was hoping someone could shed some light on some odd behaviour.

 

My code is as follows:

 

void LpTimerInit(void)
{
  /*
    DBG_EN = 1
    DOZE_EN = 1
    SW_RST = 1
    M_CEN = 1
  */
  LPIT0->MCR = 0x0000000F;

  /*
    "Before clearing the Software Reset bit, software must wait for 4
     peripheral clocks (for clock synchronization and reset propagation)."

    CPU clock is 80 MHz. SOSCDIV2_CLK is 1 MHz.
      80 MHz / 1 MHz = 80 per clock tick. 80 * 4 clock ticks = 320.
  */
  for (uint32_t i = 0; i < 320; i++)
  {
    /*
      Intentionally empty.

      Yes, this is more than 320 instructions, but this is a lazy/easy way to wait for long enough.

      Make sure code is not optimized away.
    */
  }

  /*
    SW_RST = 0: abort reset.
  */
  LPIT0->MCR &= ~0x00000002;

  /*
    Not sure if we need to wait *after* clearing reset, but if there is
    a propagation delay for making reset high, then there might be one for
    making reset low as well.
  */
  for (uint32_t i = 0; i < 320; i++)
  {
    /* Intentionally empty. */
  }

  /*
    TRG_SEL = 0
    TRG_src=0
    TROT = 0
    TSOI = 0
    TSOT = 0
    Mode = 00
    CHAIN = 0
    T_EN = 0
  */
  LPIT0->TMR[0].TCTRL = 0x00000000;
  LPIT0->TMR[1].TCTRL = 0x00000000;

  LPIT0->TMR[0].TVAL = 1000000;

  /* Just for testing. Will, of course, get a different value. */
  LPIT0->TMR[1].TVAL = 1000000; 

  /*
    TIE0 = 1: Interrupt request on channel 0
  */
  LPIT0->MIER = 0x00000001;

  /*
    Interrupt LPIT Ch0 enabled in NVIC.
  */
  enableInterrupt(LPIT0_Ch0_IRQn);

  /*
    Start channels 0 and 1 simultaneously.
  */
  LPIT0->SETTEN = 0x00000003;
}

 

 

Other details about the setup:
I'm using an 8 MHz crystal on SOSC. I'm feeding SOSC into the SPLL to generate a 160 MHz SPLL_CLK, which is divided down to an 80 MHz CORE_CLK. I divide SOSC down to a 1 MHz SOSCDIV2_CLK, which feeds the functional clock of the LPIT.

 

Everything works as expected. I can generate the 1s interrupt through ch0. However, immediately after executing the last line in the code, there is already a time difference between Ch0 and Ch1. See the following:

jh2_0-1604674024801.png

I have verified that before executing the statement, CVAL0 and CVAL1 are both still 0xFFFFFFFF. TVAL0 and TVAL1 are loaded correctly.

The time difference always comes down to 829 microseconds, and stays constant after this initial offset. This is almost a whole millisecond. I thought that setting the timers with SETTEN would cause them to start simultaneously. What could cause this behaviour I'm seeing?

0 件の賞賛
返信
1 解決策
2,948件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi jh2,

Have you tried the suggestions in S32K1xx MCU Family - Reference Manual  ?

"While the timer is running, CVALn register reads may not return the real value. If the timer value needs to be read, read it during an LPIT interrupt service routine."

48.1.5 Current timer value.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,949件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi jh2,

Have you tried the suggestions in S32K1xx MCU Family - Reference Manual  ?

"While the timer is running, CVALn register reads may not return the real value. If the timer value needs to be read, read it during an LPIT interrupt service routine."

48.1.5 Current timer value.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,943件の閲覧回数
Joey_van_Hummel
Contributor IV

Thank you. We use the S32K146. I missed the W suffix, and thought I was in the clear.

Since we need to poll the timer for exact microseconds, I'd rather not use an interrupt. I think we'll have to use the FTM for that.

0 件の賞賛
返信