The problem of files which CT configuration generate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The problem of files which CT configuration generate

5,131件の閲覧回数
Hermit
Contributor I

Hi Team

We team want to develop the project on S32K342. The version of IDE is S32DS V3.5 and the package of RTD is "SW32K3_RTD_4.4_2.0.2_DS_updatesite_D2211.zip". I attach a creenshot which shows the specific version I set up. 

When we have finished the CT configuration and updated the code, we can not build it successfully. One of attached screenshots shows the problem. And we find that the content of it is totally same with another head file. If we replace "FlexCAN_Ip_Sa_BOARD_InitPeripherals_PBcfg.h" with "FlexCAN_Ip_Sa_PBcfg.h",it can be built successfully.

Does the RTD version matter?

 

Best Regards

Hermit

0 件の賞賛
返信
2 返答(返信)

5,120件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Hermit,

Below is my test result, everything works fine.

Senlent_0-1675414717257.png

The RTD 2.0.2 FlexCAN module does not generate the file "FlexCAN_Ip_Sa_PBcfg.h".

0 件の賞賛
返信

5,093件の閲覧回数
Hermit
Contributor I

Hi Senlent

Thanks for your response.

Best Regards,

Hermit

0 件の賞賛
返信