The error of Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The error of Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library

2,021件の閲覧回数
binqin
Contributor III

I am using S32K144 development board,and I would like to use Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library. After I open the example project and compile ,the error occurred as shown in figure 1.Also,the error occurred as shown in figure 2 when I installed the license.So I only can use DOS method to obtain Host ID as shown in figure 3,but the Host ID was ae8a8. Is there any association?Can you help me solve the problem?1.jpgp12.jpgp23.jpgp3

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,758件の閲覧回数
binqin
Contributor III

Hi,

I have found the HostID was 000AE8A8,and generated a new license as shown in figure 1,but the problem wasn't solved as shown in figure 2.I think the problem may caused because of  "Index exceeds matrix dimensions." .Can you help me?

Regards,

Tony

1.pngp12.pngp2

0 件の賞賛
返信

1,758件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Discussion moved and finalized here: https://community.nxp.com/thread/451769 

0 件の賞賛
返信

1,758件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Please check the answer here: https://community.nxp.com/thread/451769#comment-907299 

Best regards,
Daniel

0 件の賞賛
返信

1,758件の閲覧回数
binqin
Contributor III

Hi Daniel,

The problem wasn't solved,can you help me to see my new reply?Thanks very much.

Regards,

Tony

0 件の賞賛
返信