Where is the MC33903 in FRDM-S32K144 EVB? What should I do about it before I use the CAN bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the MC33903 in FRDM-S32K144 EVB? What should I do about it before I use the CAN bus?

1,338 Views
maxmathew
Contributor II

 I have a S32K144 EVB board.These days I want to use CAN bus and I have read the " S32K14x Series Reference Manual". It seems that I can use CAN by configuring the register in S32K144 according to the " Reference Manual". But,the example for S32K144 in S32DS have something about "MC333903", but I can not find anything about "MC333903" in the " Reference Manual". I want to know whether I need to read other Manuals in order to use CAN bus.

Labels (1)
0 Kudos
4 Replies

977 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

There are currently two boards FRDMPK144-Q100 and S32K144EVB-Q100.

The MC33903 is a system basis chip (SBC) with CAN transceiver on FRDMPK144-Q100.

Whereas S32K144EVB-Q100 has UJA1169. Both chips are configurable via SPI.

You can configure only FlexCAN (output/input on CAN_RX, CAN_TX) using S32K144 registers. But if you need CAN interface (CAN_HI, CAN_LO) you need the SBC or other CAN transceiver.

Regards,

Daniel

0 Kudos

977 Views
maxmathew
Contributor II

My board is FRDM-S32K144. I can find TJA1050, however I can not find MC33903 or UJA1169. Should I worry about this? Can TJA1050 work as transceiver without any configuration?

0 Kudos

977 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

In case you have TJA1050 CAN transceiver on that board, you can use it without any configuration.

 

Regards,

Daniel

977 Views
maxmathew
Contributor II

Thank you very much! You have helped me solve the confusion!

0 Kudos