The error of Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The error of Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library

2,011 次查看
binqin
Contributor III

I am using S32K144 development board,and I would like to use Matlab Motor Control Toolbox for MATLAB / Simulink MBD supporting S32K1.0 library. After I open the example project and compile ,the error occurred as shown in figure 1.Also,the error occurred as shown in figure 2 when I installed the license.So I only can use DOS method to obtain Host ID as shown in figure 3,but the Host ID was ae8a8. Is there any association?Can you help me solve the problem?1.jpgp12.jpgp23.jpgp3

标签 (1)
0 项奖励
回复
4 回复数

1,748 次查看
binqin
Contributor III

Hi,

I have found the HostID was 000AE8A8,and generated a new license as shown in figure 1,but the problem wasn't solved as shown in figure 2.I think the problem may caused because of  "Index exceeds matrix dimensions." .Can you help me?

Regards,

Tony

1.pngp12.pngp2

0 项奖励
回复

1,748 次查看
Daniel_Popa
NXP Employee
NXP Employee

Discussion moved and finalized here: https://community.nxp.com/thread/451769 

0 项奖励
回复

1,748 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Please check the answer here: https://community.nxp.com/thread/451769#comment-907299 

Best regards,
Daniel

0 项奖励
回复

1,748 次查看
binqin
Contributor III

Hi Daniel,

The problem wasn't solved,can you help me to see my new reply?Thanks very much.

Regards,

Tony

0 项奖励
回复