The S32K3 chip cannot be connected using jlink, and the chip reset pin keeps resetting.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The S32K3 chip cannot be connected using jlink, and the chip reset pin keeps resetting.

196 Views
shangyuansun
Contributor I

Hi,

I encountered a problem while debugging the clock of the S32K342 chip. During the debugging phase, the J-Link suddenly disconnected, and afterward, the J-Link could not connect to the chip. I noticed that the chip's reset pin was continuously resetting. What should I do?

Regards,

shangyuansun

0 Kudos
Reply
1 Reply

163 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @shangyuansun 

Could you please provide details about the last application that was flashed onto the MCU?

Also, could you check the reset signal using an oscilloscope? Please measure the reset pin directly and share an image of the waveform you observe.

Additionally, I would recommend trying a method that has worked for me and other customers experiencing similar behavior: To flash the MCU, hold the reset line low while attempting to flash it with a simple example, like a blink application. It may fail initially and prompt you to retry. When that happens, let the reset line go high and then try flashing the program again.

Please note: These steps have only been tested on evaluation boards (EVBs), so results may vary in custom hardware.

If the issue persists after trying these steps, please let me know.

 

BR, VaneB

0 Kudos
Reply