TPPSDK(GD3000 Driver)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TPPSDK(GD3000 Driver)

1,042件の閲覧回数
ScottXing
Contributor II

Hi , Experts, we want design a BLDC controller using S32K3XX and GD3000 which can control two  BLDCs, so it need two GD3000, From the TPPSDK of GD3000's example,  I found that the CS  of SPI communication of S32K344 is controlled by SIUL2.

Now if I want to use a S32K344 to communicate with two GD3000s in a chain:

 should I change the source code of TPPSDK to make the CS conrolled by LPSPI?  

 

by the way , I want to ask you guys why the  chipselect of spi communication is designed to controlled by SIUL2/Port/Dio......?  Isn't it better if it directly controlled by LPSPI itself?

タグ(2)
0 件の賞賛
返信
1 返信

1,000件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Please refer to Application Software of MCTPTX1AK324, where it is used the TPPSDK_GD3000_Driver to control triple PMSM motors.

Such application was built and tested using the following IDE, Drivers and Tools:

- S32 Design Studio for S32 Platform Version 3.5
- S32K3xx development package version 3.5.2
- S32K3 RTD AUTOSAR 4.4 Version 2.0.0 (S32DS Extensions and Updates installation)
- FreeMASTER 3.2.1.6

Hope it helps you.

Have a nice day!

0 件の賞賛
返信