TJA1050 Library & Example Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1050 Library & Example Code

ソリューションへジャンプ
5,224件の閲覧回数
kc23
Contributor I

Hi,
Recently I have bought a TJA1050 module and wanted to connect to S32K144EVB.
Do you have an example code or library to use this module?
FYI below is the link of the website I bought the module.
(https://shopee.com.my/TJA1050-CAN-the-controller-interface-module-the-bus-driver-interface-module-i....

Thank you.

0 件の賞賛
返信
1 解決策
5,169件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I didn't find any sample code or library for TJA1050 in S32K forum or S32K EVB solution for your reference.

BR!

元の投稿で解決策を見る

4 返答(返信)
4,777件の閲覧回数
Abhaya_Raj_Mishra
Contributor I

Hi, I am using TJA1050 with TC377 for UART to CAN conversion. But not able to get any output from CAN side in PCAN software, and as well as while sending signals from PCAN side CAN (Input), but not getting any output on UART Rx.

Please help me regarding this. 

 

0 件の賞賛
返信
5,201件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I checked this module and seems like only the pin-s need to be control.

Control pin S allow two operating modes to be selected:high-speed or silent mode.

1.high-speed mode is the normal operating mode and is selected by connecting pin S to ground,It is the default mode if pin S in not connected.

2.In the silent mode, the transmitter is disabled.

so if you connect the pin-s to ground then you don't need to configurate it.

0 件の賞賛
返信
5,179件の閲覧回数
kc23
Contributor I

Hi Senlent,

Thank you for your fast reply.
Yes, I noticed that in the datasheet.

But what I would really like to know, is there any example code or library to use for this module?

Thank you.

0 件の賞賛
返信
5,170件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I didn't find any sample code or library for TJA1050 in S32K forum or S32K EVB solution for your reference.

BR!