TJA1050 Library & Example Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1050 Library & Example Code

Jump to solution
5,225 Views
kc23
Contributor I

Hi,
Recently I have bought a TJA1050 module and wanted to connect to S32K144EVB.
Do you have an example code or library to use this module?
FYI below is the link of the website I bought the module.
(https://shopee.com.my/TJA1050-CAN-the-controller-interface-module-the-bus-driver-interface-module-i....

Thank you.

0 Kudos
Reply
1 Solution
5,170 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I didn't find any sample code or library for TJA1050 in S32K forum or S32K EVB solution for your reference.

BR!

View solution in original post

4 Replies
4,778 Views
Abhaya_Raj_Mishra
Contributor I

Hi, I am using TJA1050 with TC377 for UART to CAN conversion. But not able to get any output from CAN side in PCAN software, and as well as while sending signals from PCAN side CAN (Input), but not getting any output on UART Rx.

Please help me regarding this. 

 

0 Kudos
Reply
5,202 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I checked this module and seems like only the pin-s need to be control.

Control pin S allow two operating modes to be selected:high-speed or silent mode.

1.high-speed mode is the normal operating mode and is selected by connecting pin S to ground,It is the default mode if pin S in not connected.

2.In the silent mode, the transmitter is disabled.

so if you connect the pin-s to ground then you don't need to configurate it.

0 Kudos
Reply
5,180 Views
kc23
Contributor I

Hi Senlent,

Thank you for your fast reply.
Yes, I noticed that in the datasheet.

But what I would really like to know, is there any example code or library to use for this module?

Thank you.

0 Kudos
Reply
5,171 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@kc23

I didn't find any sample code or library for TJA1050 in S32K forum or S32K EVB solution for your reference.

BR!