StandardTypes.h: No such file or directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

StandardTypes.h: No such file or directory

跳至解决方案
4,506 次查看
Silvano
Contributor I

Hello,

I have this error when I try to build the project : 

Silvano_0-1709639789376.png

 

I installed RTD version 4.0.0 to use the package for S32K396-LQFP : 

Silvano_1-1709639874763.png

I also tried to insert manually all the <file_name>.h in the includes folder from the workspace but I still have errors.

Could you help me please ?:

 

Silvano_2-1709640662945.pngSilvano_3-1709640677066.png

Silvano_0-1709641697298.png

 

 

0 项奖励
回复
1 解答
4,480 次查看
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,482 次查看
Silvano
Contributor I

Hello @spara7c5 

Yes , I am trying to compile the example project. 

I have this issue since I installed the "RTD AUTOSAR R21-11 Version 4.0.0 HF01 " and it was working normally with the version 3.0.0.

Do you think I should install EB tresos Studio 29.0.0 ?

0 项奖励
回复
4,481 次查看
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

0 项奖励
回复
4,475 次查看
Silvano
Contributor I
It was the problem, thank you!
There was a conflict between version 3.0 and 4.0
0 项奖励
回复
4,497 次查看
spara7c5
Contributor III

Hello Silvano,
I faced the same issue like you and it was for an unmatch between tresos RTD version and S32DS installed RTD. Are you trying to compile the example project? they work out of the box

0 项奖励
回复