StandardTypes.h: No such file or directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

StandardTypes.h: No such file or directory

ソリューションへジャンプ
4,502件の閲覧回数
Silvano
Contributor I

Hello,

I have this error when I try to build the project : 

Silvano_0-1709639789376.png

 

I installed RTD version 4.0.0 to use the package for S32K396-LQFP : 

Silvano_1-1709639874763.png

I also tried to insert manually all the <file_name>.h in the includes folder from the workspace but I still have errors.

Could you help me please ?:

 

Silvano_2-1709640662945.pngSilvano_3-1709640677066.png

Silvano_0-1709641697298.png

 

 

0 件の賞賛
返信
1 解決策
4,476件の閲覧回数
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,478件の閲覧回数
Silvano
Contributor I

Hello @spara7c5 

Yes , I am trying to compile the example project. 

I have this issue since I installed the "RTD AUTOSAR R21-11 Version 4.0.0 HF01 " and it was working normally with the version 3.0.0.

Do you think I should install EB tresos Studio 29.0.0 ?

0 件の賞賛
返信
4,477件の閲覧回数
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

0 件の賞賛
返信
4,471件の閲覧回数
Silvano
Contributor I
It was the problem, thank you!
There was a conflict between version 3.0 and 4.0
0 件の賞賛
返信
4,493件の閲覧回数
spara7c5
Contributor III

Hello Silvano,
I faced the same issue like you and it was for an unmatch between tresos RTD version and S32DS installed RTD. Are you trying to compile the example project? they work out of the box

0 件の賞賛
返信