Hello,
I have this error when I try to build the project :
I installed RTD version 4.0.0 to use the package for S32K396-LQFP :
I also tried to insert manually all the <file_name>.h in the includes folder from the workspace but I still have errors.
Could you help me please ?:
Solved! Go to Solution.
For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"
Hello @spara7c5
Yes , I am trying to compile the example project.
I have this issue since I installed the "RTD AUTOSAR R21-11 Version 4.0.0 HF01 " and it was working normally with the version 3.0.0.
Do you think I should install EB tresos Studio 29.0.0 ?
For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"
Hello Silvano,
I faced the same issue like you and it was for an unmatch between tresos RTD version and S32DS installed RTD. Are you trying to compile the example project? they work out of the box