Some clarification about the revision numbers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some clarification about the revision numbers?

ソリューションへジャンプ
4,336件の閲覧回数
mkdomenico
Contributor II

Hello support team,

 

I would like to ask you for some clarifications regarding the revision numbers of the datasheets and components. To this day, I have two different datasheets in my possession:

 

S32K144_RM_RevA, August 2015

S32K144 Reference Manual

S32K144_RM_Rev1, August 2016

S32K14x Series Reference Manual

 

According to the S32 production timeline however, there are two versions of the S32K144, the 1.0 and the 2.0 (and an updated 2.0), where the 2.0 is not yet available.

 

As IDE, I am using IAR but I also have S32DS on my computer. The IAR header file (S32K144.h) is at revision 1.2, referenced for:

KE1xP100M150SF0RM Rev. 0, Mar. 2015

 

In S32DS, with the IAR plugin, I have the revision 1.9, referenced for:

S32K144RM Rev. 1, Draft D, 10/2015

 

The microcontroller on the demo board I am using seems to conform to the revision A, being identified as 0N77P. Could you please tell my if the following matching table is correct?

 

Datasheets

Timeline

IAR header

Rev A

Rev 1.0

Rev 0

Rev 1

Rev 2.0

Rev 1

 

Thanks a lot,

Domenico

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
4,078件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Domenico,

 

regarding reference manual - yes, that’ correct. Rev A is for cut 1.0, Rev 1 is for cut 2.0.

S32 Design Studio v1.2 supports cut 1.0 silicon - the header file included in this version is 1.9 (that’s for cut 1.0).

S32 Design Studio v1.3 will support cut 2.0 - it will include header file for cut 2.0. It should be released this month.

 

Regards,

Lukas

元の投稿で解決策を見る

4 返答(返信)
4,079件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Domenico,

 

regarding reference manual - yes, that’ correct. Rev A is for cut 1.0, Rev 1 is for cut 2.0.

S32 Design Studio v1.2 supports cut 1.0 silicon - the header file included in this version is 1.9 (that’s for cut 1.0).

S32 Design Studio v1.3 will support cut 2.0 - it will include header file for cut 2.0. It should be released this month.

 

Regards,

Lukas

4,078件の閲覧回数
mkdomenico
Contributor II

Hi Lukas,

thanks for your answer.

Have a nice day,

Regards,

Domenico

0 件の賞賛
返信
4,078件の閲覧回数
padmanabhlanke
Contributor III

In the S32 page there is only fact sheets that do not provide information about pin-out and design specifications. So where did you find datasheet and ref.manual???

0 件の賞賛
返信
4,078件の閲覧回数
mkdomenico
Contributor II

I'd be really glad if someone could clarify this point please.

Regards,

Domenico

0 件の賞賛
返信