EAR examples problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EAR examples problem

2,688 Views
pietroserao
Contributor II

Good evening to everybody.

My name is Pietro, i'm using  S32 Design Studio for ARM Version: 1.2

I'm using an X-FRDMPK144-Q100 NXP Demoboard.

 

I'm trying to run some EAR driver examples but i can't recognize some header libraries.

The missing files are Cpu.h, pin_mux.h, clockMan1.h and flexTimer1.h 

 

 

I show you what i see

168397_168397.jpgmissing libraries.jpg

 

 

How can i find that files? There is a particular setup?

Are that examples suitable for my demoboard?

 

Thank you.

Labels (1)
0 Kudos
Reply
2 Replies

2,480 Views
raresvasile
NXP Employee
NXP Employee

Hi Pietro,

It seems that the ProcessorExpert configuration files are not generated. 

You can go in the menu bar and select Generate ProcessorExpert Code under project(Please see the attached picture below). This should generate the necessary configuration structures in order to compile the application.

pastedImage_2.png

Please let me know if this was the solution.

Thanks,

Rares

0 Kudos
Reply

2,480 Views
pietroserao
Contributor II

Thank you so much!

It works now :-)

0 Kudos
Reply