Simple PWM example[S32k144]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple PWM example[S32k144]

Jump to solution
12,239 Views
electronica2pow
Contributor III

Hi to all the community,

I am trying to configure the S32K144 platform in order to have PWM outputs from FTM0 and FTM3. Do anyone have a simple example where i can initialize the PWM and configure its frequency and duty cycle? I was reading FTMs32k144 example, but it is just an initialization of the PWM, not a real configuration.

Regards,

Jorge

Tags (1)
1 Solution
10,696 Views
danielmartynek
NXP TechSupport
NXP TechSupport
5 Replies
8,662 Views
Supertyp
Contributor I

The File AN5303SW.zip doesnt exist anymore. Please upload agin.

Im new to the S32 Universe and im stuck also at the simple PWM Output at FTM2.

0 Kudos
Reply
10,697 Views
danielmartynek
NXP TechSupport
NXP TechSupport
5,615 Views
lyz
Contributor II

Hello,

lyz_0-1699260780927.png

I Access the File AN5303SW.zip, Access Defined? As follow figure, 

lyz_0-1699260945136.png

Why? I want to get the file AN5303SW.zip.

please help me

0 Kudos
Reply
10,440 Views
EstherShokry
Contributor I

Hello Daniel

Can you send the example again because the link is damaged 

Thank you 

10,696 Views
electronica2pow
Contributor III

Thank you Daniel! It was really helpful :smileyhappy:

0 Kudos
Reply