Simple PWM example[S32k144]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Simple PWM example[S32k144]

跳至解决方案
12,242 次查看
electronica2pow
Contributor III

Hi to all the community,

I am trying to configure the S32K144 platform in order to have PWM outputs from FTM0 and FTM3. Do anyone have a simple example where i can initialize the PWM and configure its frequency and duty cycle? I was reading FTMs32k144 example, but it is just an initialization of the PWM, not a real configuration.

Regards,

Jorge

标记 (1)
1 解答
10,699 次查看
danielmartynek
NXP TechSupport
NXP TechSupport
5 回复数
8,665 次查看
Supertyp
Contributor I

The File AN5303SW.zip doesnt exist anymore. Please upload agin.

Im new to the S32 Universe and im stuck also at the simple PWM Output at FTM2.

0 项奖励
回复
10,700 次查看
danielmartynek
NXP TechSupport
NXP TechSupport
5,618 次查看
lyz
Contributor II

Hello,

lyz_0-1699260780927.png

I Access the File AN5303SW.zip, Access Defined? As follow figure, 

lyz_0-1699260945136.png

Why? I want to get the file AN5303SW.zip.

please help me

0 项奖励
回复
10,443 次查看
EstherShokry
Contributor I

Hello Daniel

Can you send the example again because the link is damaged 

Thank you 

10,699 次查看
electronica2pow
Contributor III

Thank you Daniel! It was really helpful :smileyhappy:

0 项奖励
回复