Setting up CAN driver for s32k322 using code configuration tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up CAN driver for s32k322 using code configuration tool

Jump to solution
6,721 Views
pratik_a
Contributor III

Hi,

I'm trying to configure CAN1 which is PTC8 and PTC9 of S32k322 as a CAN transceiver.  As can be seen in image 1.png I have included the necessary components. After updating the code I'm getting the following 5 errors,

Error 1:

workspaceS32DS.3.5\trial21_02_24\trial21_02_24_M7_1\Debug_FLASH/../RTD/src/Can_43_FLEXCAN.c:1135: undefined reference to `CanIf_ControllerModeIndication'

Error 2: 

s32ds.3.5/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/bin/real-ld.exe: workspaceS32DS.3.5\trial21_02_24\trial21_02_24_M7_1\Debug_FLASH/../RTD/src/Can_43_FLEXCAN.c:1184: undefined reference to `CanIf_ControllerModeIndication'

Error 3:

workspaceS32DS.3.5\trial21_02_24\trial21_02_24_M7_1\Debug_FLASH/../RTD/src/Can_43_FLEXCAN.c:2997: undefined reference to `CanIf_ControllerBusOff'

Error 4:

workspaceS32DS.3.5\trial21_02_24\trial21_02_24_M7_1\Debug_FLASH/../RTD/src/Can_43_FLEXCAN_Ipw.c:2613: undefined reference to `CanIf_ControllerModeIndication'

Error 5:

make: *** [makefile:39: trial21_02_24_M7_1.elf] Error 1

 

Any help is appreciated.

Thanks, in advance.

0 Kudos
Reply
1 Solution
6,622 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @pratik_a,

Please try declaring the functions in your main code for your application, just like in the example:

void CanIf_ControllerBusOff(uint8 ControllerId)
{
    (void)ControllerId;
}

void CanIf_ControllerModeIndication(uint8 ControllerId, Can_ControllerStateType ControllerMode )
{
    (void)ControllerId;
    (void)ControllerMode;
}

Best regards,
Julián

View solution in original post

4 Replies
6,585 Views
pratik_a
Contributor III

Hi @Julián_AragónM 

It worked. Thanks

6,705 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @pratik_a,

Firstly, could you share the version of the RTD package you are using? 

Could you also share how did you create the project? Is this from scratch or are you basing this application off of the Can_Example from the RTD? 

Please confirm you are including the necessary file for the driver, as shown in the example (this is not made automatically with the "UpdateCode" button):

 

#include "Can_43_FLEXCAN.h"

 

Best regards,
Julián

0 Kudos
Reply
6,686 Views
pratik_a
Contributor III

Hi @Julián_AragónM 

Thank you for the response.

I'm creating the project from scratch. I selected the controller NXP S32k322 along with SDK named PlatformSDK_S32K3_S32K322_M7_0 version 3.0.0 refer image 1.png and included the modules directly from the components section as can be seen in image 2.png

I also tried including the header file in main.c

#include "Can_43_FLEXCAN.h"

The error still persists.

Best regards,

Pratik 

0 Kudos
Reply
6,623 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @pratik_a,

Please try declaring the functions in your main code for your application, just like in the example:

void CanIf_ControllerBusOff(uint8 ControllerId)
{
    (void)ControllerId;
}

void CanIf_ControllerModeIndication(uint8 ControllerId, Can_ControllerStateType ControllerMode )
{
    (void)ControllerId;
    (void)ControllerMode;
}

Best regards,
Julián