[Security]porting security to APP but loop in (FALSE == Mu_Ip_IsResponseReady)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Security]porting security to APP but loop in (FALSE == Mu_Ip_IsResponseReady)

ソリューションへジャンプ
1,987件の閲覧回数
faiz_gear
Contributor II

We are using S32K312,and the HSE function is running successful in FBL.

Now we want to porting the security for FBL to APP,but we find is loop in

while ((FALSE == Mu_Ip_IsResponseReady(Hse_Ip_apMuBase[u8MuInstance], u8MuChannel)) && (u32ElapsedTicks < u32TimeoutTicks))

in Hse_Ip_ServiceRequest when we call the Hse service.

But it is all right in FBL.I want to konw what may causes the HSE to be unresponsive?

タグ(2)
0 件の賞賛
返信
1 解決策
1,768件の閲覧回数
WeoWang
NXP Employee
NXP Employee

Hi David,

If you call the HSE service asynchronously, and you have the debugger attached to the MCU, you can try to remove the debugger and add a message print(via CAN or UART) or toggle an LED after this function

while ((FALSE == Mu_Ip_IsResponseReady(Hse_Ip_apMuBase[u8MuInstance], u8MuChannel)) && (u32ElapsedTicks < u32TimeoutTicks))

We found that sometimes the interrupts could not be entered when the debugger was attached.

You can also check whether the related interrupts are enabled or not:

WeoWang_0-1723693222001.png

 

Best Regards

WW

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,849件の閲覧回数
David2024
Contributor II

Hi:

    I met the same problem as you, if you have solved this problem, can you share the solution with  me, thanks very much!

0 件の賞賛
返信
1,769件の閲覧回数
WeoWang
NXP Employee
NXP Employee

Hi David,

If you call the HSE service asynchronously, and you have the debugger attached to the MCU, you can try to remove the debugger and add a message print(via CAN or UART) or toggle an LED after this function

while ((FALSE == Mu_Ip_IsResponseReady(Hse_Ip_apMuBase[u8MuInstance], u8MuChannel)) && (u32ElapsedTicks < u32TimeoutTicks))

We found that sometimes the interrupts could not be entered when the debugger was attached.

You can also check whether the related interrupts are enabled or not:

WeoWang_0-1723693222001.png

 

Best Regards

WW

0 件の賞賛
返信
1,841件の閲覧回数
faiz_gear
Contributor II

please check the address of data that you want to send to HSE,It should be in sram data or dtcm

0 件の賞賛
返信
1,659件の閲覧回数
FHY
Contributor I
Hi faiz_gear,
I encountered the same problem. Have you found a solution. Is it necessary to perform some configuration operations before using HSE capabilities? Could you please share the specific solution? Thank you very much.
0 件の賞賛
返信