Security algorithm(ECC, SHA 256, SM2 ,SM3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security algorithm(ECC, SHA 256, SM2 ,SM3)

1,464 Views
FangSheng
Contributor I

Hello

Currently, we are developing security programming based on S32K148. Is there an SDK source filr or algorithm library that supports the following algorithms and some example programs for this chip.
If not, is there a practice to compile the algorithm library based on the Openssl source file.

We look forward to your reply. 

International cryptographic algorithm :ECC, SHA 256

Chinese commercial cryptographic algorithm:  SM2 ,SM3

Regards.

0 Kudos
Reply
1 Reply

1,449 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm sorry, I'm afraid we can't help here. We do not provide supporting materials for this. It's completely up to users to implement such SW features.

Regards,

Lukas

0 Kudos
Reply