Security algorithm(ECC, SHA 256, SM2 ,SM3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Security algorithm(ECC, SHA 256, SM2 ,SM3)

1,486件の閲覧回数
FangSheng
Contributor I

Hello

Currently, we are developing security programming based on S32K148. Is there an SDK source filr or algorithm library that supports the following algorithms and some example programs for this chip.
If not, is there a practice to compile the algorithm library based on the Openssl source file.

We look forward to your reply. 

International cryptographic algorithm :ECC, SHA 256

Chinese commercial cryptographic algorithm:  SM2 ,SM3

Regards.

0 件の賞賛
返信
1 返信

1,471件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm sorry, I'm afraid we can't help here. We do not provide supporting materials for this. It's completely up to users to implement such SW features.

Regards,

Lukas

0 件の賞賛
返信