STCU2 and FCC interactions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

STCU2 and FCC interactions

跳至解决方案
2,804 次查看
FabioG
Contributor III

Hi There,

Reading User Manual i have understood that, please confirm or not (and, please, explain, if not):

1) Unrecoverable faults are configurable by the apposite ST32 studio Bist window (in peripherial view), isn't it?

3) Unrecoverable faults set  STRU2_ERR.UFSF bit  and a destructive reset reaction, isn't it?

4) Recoverable faults  set STRU2_ERR.RFSF and triggers one of FCCU NCF5 group of faults, Isn't it?

5) in user manual, in STCU2_ERR description, it is said  that also an unrecoverable fault, STRU2_ERR.UFSF=1, triggers FCCU, why? does it also triggers NCF5 group?

6) If SPD Bist_Run(BIST_SAFETYBOOT_CFG) is done prior to configure  FCCU, at init phases, STRU2_ERR.RFSF is set but FCCU is not triggered, because it is not initializad yet, isn't it?

7) To validate STRU2_ERR.RFSF path is it  necessary to inject in FCCU.NCFF one of the NCF5 fault numbers, for example, EMCEM_DCM_NCF_5_FAULT_MONITOR0 = 1, isnt'it ?

if it is injected EMCEM_DCM_NCF_5_FAULT_MONITOR0 = 1 in FCCU_NCFF is also set STRU2_ERR.RFSF for testing it  ?

Best Regards,

Fabio

0 项奖励
回复
1 解答
2,748 次查看
RadoslavB
NXP Employee
NXP Employee

Yes you can use  eMcem_InjectFault() for fake fault injection into FCCU.
Reaction path can be tested by observing desired reaction:
- jump into Alarm interrupt handler (R1)
- jump into NMI (R1)
- triggering functional reset (R3)
- EOUT signaling in addition to R2 or R3

You can also use sCheck FCCU_NCF check, this is available in Premium SAF.


Kind Regards,
Radoslav

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,764 次查看
RadoslavB
NXP Employee
NXP Employee

Hi Fabio,

ad 1)
Yes in the BIST configuration - Unrecoverable MBIST/LBIST tabs, you can set which LBIST/MBIST will be handled as unrecoverable.

ad 3)
Yes correct.

ad 4)
Yes, it sets the STCU2_ERR.RFSF flag and sets status flag for the NCF_5 channel – based on the NCF_5 channel setting it performs desired reaction.

ad 5)
Unrecoverable STCU2 faults don't trigger FCCU, there is a note in the RM:

radoslavbogusz_0-1709070564120.pngradoslavbogusz_0-1709070564120.png

ad 6)
Correct, by default after the reset FCCU NCF channels are disabled.
If you want to utilize FCCU reporting path or EOUT signaling from STCU2 please execute eMcem_init() beforehand.

ad 7)
STCU2 has no fault injection mechanism, you can only inject desired NCF_DCM fault ID and test the reaction path within FCCU.
ERRSTAT RFSF bit is not set when injecting fault into FCCU, this bit can’t be set by any fake injection.
STCU2 itself is mechanism to check latent faults in other peripherals or memories on the chip, checking latent faults in STCU2 (i.e. check latent faults in the HW STCU2 checker for checking other MCU latent faults) is beyond the scope of the metrics required by FuSa standards (that would lead to never-ending  chain of check of the checkers).

 


Kind Regards,
Radoslav

0 项奖励
回复
2,754 次查看
FabioG
Contributor III

At point 7 you say

"STCU2 has no fault injection mechanism, you can only inject desired NCF_DCM fault ID and test the reaction path within FCCU."

I suppose this is performed by a fake fault injection in FCCU.NCFF (correct)? so, How  can I check the "test rection path" you refer to ? How can I understand if the reaction path test result is correct, (after a FCCU.NCFF, NCF_DCM bit set)?

Best Regards,

Fabio 

 

0 项奖励
回复
2,749 次查看
RadoslavB
NXP Employee
NXP Employee

Yes you can use  eMcem_InjectFault() for fake fault injection into FCCU.
Reaction path can be tested by observing desired reaction:
- jump into Alarm interrupt handler (R1)
- jump into NMI (R1)
- triggering functional reset (R3)
- EOUT signaling in addition to R2 or R3

You can also use sCheck FCCU_NCF check, this is available in Premium SAF.


Kind Regards,
Radoslav

0 项奖励
回复