SPI config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI config

810 Views
vignesh3
Contributor II

Hi NXP community,

I am working on SPI protocol to R/W SD card.

I am using bare metal code from S32K1xx cookbook, I have found this doze mode bit in CR register.

Can anyone please tell me what is this bit will do exactly if I am enabling it.

I have referred  RM, Still I can not clear myself.

 

vignesh3_0-1750768934692.png

vignesh3_1-1750769107275.png

 

 

0 Kudos
Reply
2 Replies

791 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @vignesh3 

Peripheral Doze mode is a low-power feature that allows certain peripherals to remain active while the CPU is in a low-power state. 

This topic has been discussed in other threads as well. I recommend reviewing those discussions, as they may provide additional insights that could be helpful.

How is the Doze mode working in S32K series

Low power and Doze Mode question in S32K

What is the role of DOZE mode of many modules

 

BR, VaneB

0 Kudos
Reply

773 Views
vignesh3
Contributor II
Thanks for the reply
0 Kudos
Reply