SPI config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI config

834件の閲覧回数
vignesh3
Contributor II

Hi NXP community,

I am working on SPI protocol to R/W SD card.

I am using bare metal code from S32K1xx cookbook, I have found this doze mode bit in CR register.

Can anyone please tell me what is this bit will do exactly if I am enabling it.

I have referred  RM, Still I can not clear myself.

 

vignesh3_0-1750768934692.pngvignesh3_0-1750768934692.png

vignesh3_1-1750769107275.pngvignesh3_1-1750769107275.png

 

 

0 件の賞賛
返信
2 返答(返信)

815件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @vignesh3 

Peripheral Doze mode is a low-power feature that allows certain peripherals to remain active while the CPU is in a low-power state. 

This topic has been discussed in other threads as well. I recommend reviewing those discussions, as they may provide additional insights that could be helpful.

How is the Doze mode working in S32K series

Low power and Doze Mode question in S32K

What is the role of DOZE mode of many modules

 

BR, VaneB

0 件の賞賛
返信

797件の閲覧回数
vignesh3
Contributor II
Thanks for the reply
0 件の賞賛
返信