SPI config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI config

831 次查看
vignesh3
Contributor II

Hi NXP community,

I am working on SPI protocol to R/W SD card.

I am using bare metal code from S32K1xx cookbook, I have found this doze mode bit in CR register.

Can anyone please tell me what is this bit will do exactly if I am enabling it.

I have referred  RM, Still I can not clear myself.

 

vignesh3_0-1750768934692.pngvignesh3_0-1750768934692.png

vignesh3_1-1750769107275.pngvignesh3_1-1750769107275.png

 

 

0 项奖励
回复
2 回复数

812 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @vignesh3 

Peripheral Doze mode is a low-power feature that allows certain peripherals to remain active while the CPU is in a low-power state. 

This topic has been discussed in other threads as well. I recommend reviewing those discussions, as they may provide additional insights that could be helpful.

How is the Doze mode working in S32K series

Low power and Doze Mode question in S32K

What is the role of DOZE mode of many modules

 

BR, VaneB

0 项奖励
回复

794 次查看
vignesh3
Contributor II
Thanks for the reply
0 项奖励
回复