SPI Unexpected data bits seen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Unexpected data bits seen

Jump to solution
1,295 Views
beginner100
Contributor II

Using S32K312 EVB as master, I’m sending commands with a register address and certain data configured for the Slave.

A snippet of the CS(yellow), CLK(blue), MOSI(pink), MISO(green) is below.

The MOSI(Pink) in the picture is Reg addr 07h,  Data is 20h (32 dec)

I don’t understand the other pulse when the CS is high, can you let me know what it could be? I just want to confirm if everything looks okay on the scope snippet I sent or if I should be configuring anything on the S32CT.

I have used an SPI example with LPSPI2 as Master.

 

schitta_0-1750182670588.jpeg

 

MISO(green) - no response currently seen from the Slave

schitta_1-1750182670612.jpeg

 

 

0 Kudos
Reply
1 Solution
1 Reply
1,268 Views
danielmartynek
NXP TechSupport
NXP TechSupport