SPD BIST_DIAGNOSTIC_CFG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPD BIST_DIAGNOSTIC_CFG

Jump to solution
1,478 Views
FabioG
Contributor III

Hi there,

is it possible to run Bist_Run( BIST_DIAGNOSTIC_CFG ) at boot and not BIST_SAFETYBOOT_CFG ?

In our application there is no poweron timing costraints, so the 10ms execution time of the full featured Bist  "BIST_DIAGNOSTIC_CFG" is not a problem.

Also, off chip FS26 doesn't reset the onboard and at boot time there are all the "garage" conditions required.

Finally in pre defined "parking"(for example) conditions we reset ECU in order to perform BIST_DIAGNOSTIC_CFG.

Best regards,

Fabio 

0 Kudos
Reply
1 Solution
1,442 Views
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved

View solution in original post

0 Kudos
Reply
1 Reply
1,443 Views
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved

0 Kudos
Reply