SPD BIST_DIAGNOSTIC_CFG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPD BIST_DIAGNOSTIC_CFG

跳至解决方案
1,490 次查看
FabioG
Contributor III

Hi there,

is it possible to run Bist_Run( BIST_DIAGNOSTIC_CFG ) at boot and not BIST_SAFETYBOOT_CFG ?

In our application there is no poweron timing costraints, so the 10ms execution time of the full featured Bist  "BIST_DIAGNOSTIC_CFG" is not a problem.

Also, off chip FS26 doesn't reset the onboard and at boot time there are all the "garage" conditions required.

Finally in pre defined "parking"(for example) conditions we reset ECU in order to perform BIST_DIAGNOSTIC_CFG.

Best regards,

Fabio 

0 项奖励
回复
1 解答
1,454 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,455 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved

0 项奖励
回复