SIM display "??"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SIM display "??"

1,666 Views
814420552
Contributor III

Hi

 why the following EEERAMSIZE  & DEPART  display "??"  when debug the example code ?

pastedImage_1.png

0 Kudos
Reply
5 Replies

1,588 Views
814420552
Contributor III

Dear Alexis,

      MCU:S32K146, thank you!

0 Kudos
Reply

1,588 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui,

If you want to check these two registers you would need an example that configures these two sections, for example in the SDK, there's an example called flash_partitioning that configures these two registers:

pastedImage_1.png

Also, I don't recognize this interface that you're using, are you using the latest S32 Design Studio?

Best Regards,

Alexis Andalon

0 Kudos
Reply

1,588 Views
814420552
Contributor III

    hello Alexis, 

               MCU is S32K146,

                but when debug, register FCFG1 can't display. I don't know why it is so!

pastedImage_1.png

0 Kudos
Reply

1,588 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui Wu,

Only to check, could you try updating to the latest S32DS version? I see that you're using the 2018 and there's a new one available in the following link.

Best Regards,

Alexis Andalon

0 Kudos
Reply

1,588 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui,

Can you let me know which device are you using?

Best Regards,

Alexis Andalon

0 Kudos
Reply