SDK Function execution times?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK Function execution times?

1,283 Views
JeorgeB
Contributor III

Hi.

is there any document which give SDK Function execution times?

e.g. in Flash driver and the follow function -> "FLASH_DRV_Program"

 

Thanks.

0 Kudos
Reply
1 Reply

1,273 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JeorgeB,

Please refer: Measure the running time of one function on S32K
The unit of measurements of the variabile ARM_CM_DWT_CYCCNT is CORE_CLK cycles.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply