S32k344'Rtc wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k344'Rtc wake up

Jump to solution
11,583 Views
luyq
Contributor III

Hello

 I have tested the S32k344's Rtc wake up.And i find only set to 1S to wake up,other can not.Could you help me?

Thanks.

0 Kudos
Reply
1 Solution
11,530 Views
Jeremy_He
NXP Employee
NXP Employee

Hi Lu, 

Please see the attached S32K3 standby RTC wakeup demo Build on S32K3EVB and S32K344-WB with RTD LLD 0.9.0 and S32DS3.4.  In this example, it was set to 5s wakeup period by RTC instead of API. For more details please see the readme.txt.

 

Best wishes.

Jeremy He

 

View solution in original post

12 Replies
7,213 Views
AbdNxp
Contributor II
SysStatus_t RTCInit(void)
{
Rtc_Ip_TimedateType defaultTimeDate = {1970,1,1,0,0,0};
 
NVIC_SetPriority(RTC_IRQn,2);
Rtc_Ip_Init(0, &RTC_0_InitConfig_PB_BOARD_InitPeripherals);
RTCDate_t dateNow = RTCGetDate();
if( defaultTimeDate.year > dateNow.year &&
defaultTimeDate.month > dateNow.month &&
defaultTimeDate.day > dateNow.day)
{
Rtc_Ip_SetTimeDate(0,&defaultTimeDate);
}
 
Rtc_Ip_EnableInterrupt(0,RTC_IP_COUNTER_INTERRUPT);
Rtc_Ip_StartCounter(0);
return SYS_SUCCESS;
}
I am trying to use RTC in S32K344.
above is my init function.
clock is enabled with clk src0
freeze mode enabled.
This issue is I do not see in increment in time even if the counter is ebabled.
0 Kudos
Reply
11,531 Views
Jeremy_He
NXP Employee
NXP Employee

Hi Lu, 

Please see the attached S32K3 standby RTC wakeup demo Build on S32K3EVB and S32K344-WB with RTD LLD 0.9.0 and S32DS3.4.  In this example, it was set to 5s wakeup period by RTC instead of API. For more details please see the readme.txt.

 

Best wishes.

Jeremy He

 

9,494 Views
GiangHM
Contributor I

Hi ,

Do you have example using RTD MCAL ?

0 Kudos
Reply
9,464 Views
Jeremy_He
NXP Employee
NXP Employee

Hi

Please refer to the attachment project configured by EB tresos and RTD2.0.0 version.

 

 

Best Regards,

Jeremy

0 Kudos
Reply
6,918 Views
Cppppy
Contributor II
Hi, what is the RTC wakeup time for this mcal project? Is there a corresponding S32DS project I can refer to?
0 Kudos
Reply
9,456 Views
GiangHM
Contributor I

I am using S32DS tool to config. Do you have other  project using both mcal and S32DS tool?  I want to open config file to see configuration of MCU module.

0 Kudos
Reply
9,438 Views
Jeremy_He
NXP Employee
NXP Employee

Hi

 

Do you mean config MCAL with S32CT(RTD High Level Driver)? Currently we don't have this, may add it in the future.

 

Best Regards,

Jeremy

0 Kudos
Reply
10,109 Views
WXM
Contributor II
Hello, there is a routine to wake up S32K344 by GPIO, using EB tool configuration routine
0 Kudos
Reply
10,683 Views
1260784871
Contributor II

1260784871_0-1661318411008.png

 

0 Kudos
Reply
11,526 Views
luyq
Contributor III

Ok,thanks.

Tags (1)
0 Kudos
Reply
11,570 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi luyq,

If you configure RTCVAL to 1s, then you may need to modify APIVAL and use RTC API wakeup.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
11,566 Views
luyq
Contributor III

I originally used APIVAL,but it doesn't work.

0 Kudos
Reply