S32k344'Rtc wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
11,538件の閲覧回数
luyq
Contributor III

Hello

 I have tested the S32k344's Rtc wake up.And i find only set to 1S to wake up,other can not.Could you help me?

Thanks.

0 件の賞賛
返信
1 解決策
11,485件の閲覧回数
Jeremy_He
NXP Employee
NXP Employee

Hi Lu, 

Please see the attached S32K3 standby RTC wakeup demo Build on S32K3EVB and S32K344-WB with RTD LLD 0.9.0 and S32DS3.4.  In this example, it was set to 5s wakeup period by RTC instead of API. For more details please see the readme.txt.

 

Best wishes.

Jeremy He

 

元の投稿で解決策を見る

12 返答(返信)
7,168件の閲覧回数
AbdNxp
Contributor II
SysStatus_t RTCInit(void)
{
Rtc_Ip_TimedateType defaultTimeDate = {1970,1,1,0,0,0};
 
NVIC_SetPriority(RTC_IRQn,2);
Rtc_Ip_Init(0, &RTC_0_InitConfig_PB_BOARD_InitPeripherals);
RTCDate_t dateNow = RTCGetDate();
if( defaultTimeDate.year > dateNow.year &&
defaultTimeDate.month > dateNow.month &&
defaultTimeDate.day > dateNow.day)
{
Rtc_Ip_SetTimeDate(0,&defaultTimeDate);
}
 
Rtc_Ip_EnableInterrupt(0,RTC_IP_COUNTER_INTERRUPT);
Rtc_Ip_StartCounter(0);
return SYS_SUCCESS;
}
I am trying to use RTC in S32K344.
above is my init function.
clock is enabled with clk src0
freeze mode enabled.
This issue is I do not see in increment in time even if the counter is ebabled.
0 件の賞賛
返信
11,486件の閲覧回数
Jeremy_He
NXP Employee
NXP Employee

Hi Lu, 

Please see the attached S32K3 standby RTC wakeup demo Build on S32K3EVB and S32K344-WB with RTD LLD 0.9.0 and S32DS3.4.  In this example, it was set to 5s wakeup period by RTC instead of API. For more details please see the readme.txt.

 

Best wishes.

Jeremy He

 

9,449件の閲覧回数
GiangHM
Contributor I

Hi ,

Do you have example using RTD MCAL ?

0 件の賞賛
返信
9,419件の閲覧回数
Jeremy_He
NXP Employee
NXP Employee

Hi

Please refer to the attachment project configured by EB tresos and RTD2.0.0 version.

 

 

Best Regards,

Jeremy

0 件の賞賛
返信
6,873件の閲覧回数
Cppppy
Contributor II
Hi, what is the RTC wakeup time for this mcal project? Is there a corresponding S32DS project I can refer to?
0 件の賞賛
返信
9,411件の閲覧回数
GiangHM
Contributor I

I am using S32DS tool to config. Do you have other  project using both mcal and S32DS tool?  I want to open config file to see configuration of MCU module.

0 件の賞賛
返信
9,393件の閲覧回数
Jeremy_He
NXP Employee
NXP Employee

Hi

 

Do you mean config MCAL with S32CT(RTD High Level Driver)? Currently we don't have this, may add it in the future.

 

Best Regards,

Jeremy

0 件の賞賛
返信
10,064件の閲覧回数
WXM
Contributor II
Hello, there is a routine to wake up S32K344 by GPIO, using EB tool configuration routine
0 件の賞賛
返信
10,638件の閲覧回数
1260784871
Contributor II

1260784871_0-1661318411008.png

 

0 件の賞賛
返信
11,481件の閲覧回数
luyq
Contributor III

Ok,thanks.

タグ(1)
0 件の賞賛
返信
11,525件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi luyq,

If you configure RTCVAL to 1s, then you may need to modify APIVAL and use RTC API wakeup.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
11,521件の閲覧回数
luyq
Contributor III

I originally used APIVAL,but it doesn't work.

0 件の賞賛
返信