S32k144 timer interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k144 timer interrupt

4,641件の閲覧回数
abderrahimjamao
Contributor III

Hello,

Is it possible to generate 1ms  timer interrupts using s32k144 micro?

ラベル(1)
タグ(1)
1 返信

4,571件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ABDERRAHIM JAMAOUI,

Several timers can be used to generate 1ms interrupt.

User Manuals S32K1xx SDK RTM 3.0.0 with Patch 3.0.2 for ARM.png
You can refer the modification of lpit_periodic_interrupt_s32k144.

lpit_periodic_interrupt_s32k144.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------