S32K3xx - UDS over CAN Stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3xx - UDS over CAN Stack

2,997件の閲覧回数
ASN7
Contributor III

Is there any UDS Stack over CAN available for S32K3xx series already ? 

I currently have S32K314 and I want to implement the complete the UDS Stack over CAN Bus. So I wanted to confirm if the stack is available ? 

タグ(5)
0 件の賞賛
返信
3 返答(返信)

2,979件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ASN7,

Currently, this is the only UDS example available: Unified bootloader Demo - NXP Community.

It is an UDS bootloader solution of S12Z, S32K1xx and S32K3xx.

Best regards,
Julián

0 件の賞賛
返信

2,968件の閲覧回数
ASN7
Contributor III

Hello @Julián_AragónM ,

 

I did download the latest release from the GitHub Page and I can use the ECU-BUS, but that is just to send UDS Requests via PCAN right ? I will not be able to generate code for S32K314 right or have I understood the tool incorrectly ? 

0 件の賞賛
返信

2,958件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ASN7,

but that is just to send UDS Requests via PCAN right ?  I will not be able to generate code for S32K314 right or have I understood the tool incorrectly ? 

Yes, that is correct. This is simply a reference example which can be used with the S32K family.

Best regards,
Julián

0 件の賞賛
返信