S32K3xx TCPIP_STACK Installation Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3xx TCPIP_STACK Installation Issue

2,478件の閲覧回数
khaihm
Contributor I

Hi,

We are using the S32K3X4EVB-T172 Evaluation Board and We are trying to import, build and run
TCPIP stack example.

I followed in Release Note to install the TCPIP files(SW32K3_TCPIP_1_0_3_D2306_updatesite.zip) But im facing the below issue.

"TCPIP_STACK_S32K3 Will be not installed"

Cannot complete the install because one or more required items could not be found.
Software being installed: TCPIP_STACK S32K3 1.0.3.202306190957 (com.nxp.TCPIP_STACK.S32K3.root.1.0.3.feature.feature.group 1.0.3.202306190957)
Missing requirement: RTD S32K396 3.0.0.202303311831 (com.nxp.RTD.S32K396.root.feature.feature.group 3.0.0.202303311831) requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.s32k396.dev.feature.feature.group 1.0.0' but it could not be found
Cannot satisfy dependency:
From: TCPIP_STACK S32K3 1.0.3.202306190957 (com.nxp.TCPIP_STACK.S32K3.root.1.0.3.feature.feature.group 1.0.3.202306190957)
To: org.eclipse.equinox.p2.iu; com.nxp.RTD.S32K396.root.feature.feature.group 0.0.0

Screenshot 2023-08-23 100615.png

Please help me to solve this issue.

2 返答(返信)

2,429件の閲覧回数
khaihm
Contributor I

I found the same issue in this: Solved: Re: tcpip 1.0.3 can't be installed - NXP Community

I followed in that link above and I fixed it. 

0 件の賞賛
返信

2,425件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the delay. I am glad to hear that you fixed it.

0 件の賞賛
返信