S32K3X4EVB-Q172 Debug Connector cable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3X4EVB-Q172 Debug Connector cable

ソリューションへジャンプ
3,128件の閲覧回数
joohau
Contributor II

I want to connect a Segger debugger (0.1" 20-pin Standard ARM debug connector) to the S32K3X4EVB-Q172 evalution board. This board only has a 20-pin Cortex Debug ETM+Trace connector (0.05'' 20-pin FTSH header).

Can you suggest an adapter/cable that I can use for this? The adapter from Segger (https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/) does match the pin-out but contains a dead-pin (they also call it a 19-pin adapter):

Which cable/adapter can I use to connect a debugger to the S32K3X4EVB-Q172?

1 解決策
3,071件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Joost,

this should work, you just need to remove the dead-pin to be able to plug it in.

I use something similar (LA-3500 + LA7844 + these converters LA-3770) and there was also the same dead-pin which I removed:

lukaszadrapa_0-1653050964717.png

 

Regards,

Lukas

元の投稿で解決策を見る

1 返信
3,072件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Joost,

this should work, you just need to remove the dead-pin to be able to plug it in.

I use something similar (LA-3500 + LA7844 + these converters LA-3770) and there was also the same dead-pin which I removed:

lukaszadrapa_0-1653050964717.png

 

Regards,

Lukas