Hello,
We have newly ordered S32K396-BGA-DC1 Eval Boards & trying out the basic steps given in the link : Getting Started With S32K396-BGA-DC1 Evaluation Board | NXP Semiconductors
Below are the settings that we have made
1. We are using on-board FS26 power to the uC. Hence J4, J6, J7 are connected to 2-4 positions
2. We are using on-board OpenSDA debugger. Hence J16, J17, J18 & J19 are connected to 1-2 position.
3. We have powered through the DC adapter provided in the kit & then finally turned-on the SW10
We are seeing that D1, D2, D3 & D4 LEDs are glowing. Apart from that D11(Red LED) is glowing as well.
Is this expected? When we saw the schematics, it says the FCCU1 connection coming from the uC to the PMIC. So, is it the correct state & after programming it goes away?
Thanks.