s32k312 I2C Clock Source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k312 I2C Clock Source

ソリューションへジャンプ
1,050件の閲覧回数
Hoon
Contributor III

Hi

 

I used S32K312 and there is a problem to select I2C Clock Source

Even though i set the clock source to 30Mhz and active, i2c clcok source candidates are not identified when i set i2c peripheral.

candidate group of SPI could selected without any problems, can you help me?

 

MCU : S32K312NHT0MPASR

IDE : Design Studio 3.6.2

RTD : S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 (Latest by current standards)

0 件の賞賛
返信
1 解決策
1,023件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It looks similar to the previous question, please refer to the screenshot in that question: s32k312 I2C Clock Source

Please add Clock_Ip_ReferencePoints in Peripherals tool and configure AIPS_SLOW_CLK as the MODULE_CLK source of LPI2C.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,024件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It looks similar to the previous question, please refer to the screenshot in that question: s32k312 I2C Clock Source

Please add Clock_Ip_ReferencePoints in Peripherals tool and configure AIPS_SLOW_CLK as the MODULE_CLK source of LPI2C.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信