S32K358: eDMA Trigger via GMAC PPS Module for Media Clock Generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358: eDMA Trigger via GMAC PPS Module for Media Clock Generation

251 Views
sathishkumar_sunmugavel
Contributor III

Hi Everyone,

I'm working on media clock generation using the GMAC PPS module and plan to use eDMA to update the target time (seconds and nanoseconds) dynamically. Here's a summary of my approach:


Implementation Overview:

  1. The GMAC PTP reference clock is configured at 125 MHz, which starts the system time.

  2. The Target Time Seconds and Nanoseconds registers are updated to generate a pulse every second.

  3. PPS is configured in Media Clock Generation (MCGR) mode, which should assert the mcgr_dma_req_o signal.

  4. I selected DMAMUX source 28 – “IEEE 1588 PTP timer ch[0]”, assuming it maps to mcgr_dma_req_o[0] and thus triggers an eDMA peripheral request.

  5. The TCD is set up to copy the next target time when triggered.


Observed Behavior:

  • When the system time reaches or exceeds the configured target time, the TSTARGT0 bit in the MAC_Timestamp_Status register is correctly set — indicating that mcgr_dma_req_o[0] is asserted.

    sathishkumar_sunmugavel_0-1753867248257.png

     

  • However, no DMA transfer is triggered; the current iteration count remains unchanged.


Questions:

  1. Is this method valid for generating periodic clock pulses using the PPS module and eDMA?

  2. Is the DMAMUX configuration (source 28: IEEE 1588 PTP timer ch[0]) correct for this scenario?

  3. Does the assertion of mcgr_dma_req_o actually trigger an eDMA peripheral request?

  4. The naming conventions seem inconsistent across resources:

    • DMAMUX sheet: IEEE 1588 PTP timer ch[i]

    • Reference Manual: mcgr_dma_req_o[i]

    • SDK Code: DMA_MUX_1_GMAC_0_PTP_TIMER_CH[i]


Conclusion:

I would like to confirm: when the system time meets the configured target time, the mcgr_dma_req_o signal is asserted — is this signal routed to eDMA as a valid peripheral request?

I have attached the sample main.c file for reference. Please have a look and let me know what is going wrong.

Any insights would be greatly appreciated.

Best Regards,
Sathish.

Tags (1)
0 Kudos
Reply
1 Reply

215 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @sathishkumar_sunmugavel 

I recommend to discuss this directly with NXP FAE assigned to Harman. Or you can create new case here:

https://support.nxp.com/s/?language=en_US

... and the case will be forwarded to local FAE team. 

Thanks for understanding. 

Regards,

Lukas