Hi
1st. Could you please check the state of PRTN1_COFB1_CLKEN. BLOCK53(FXOSC) and PRTN1_COFB1_CLKEN. BLOCK56(PLL) before calling Mcu_PerformReset()?
2nd. Did you configure PLL CLK or not? These two bits may impact the reset reason after the functional reset is triggered when either of the two bits are disabled and PLL is enabled.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------