S32K344 RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 RTC

1,996件の閲覧回数
S3RD4R
Contributor I

 

Hello all,

I am currently using S32K344 with MCAL libraries. I can succesfully generate interrupt for every seconds however my main purpose is to set and read time and i can not find the commands to do the trick. 

Is there any example of reading and setting time using MCAL functions?

 

My other question is: Does the device reset RTC domain when device is resetted or the device keeps on counting the RTC?

Thank you,

 

0 件の賞賛
返信
2 返答(返信)

1,573件の閲覧回数
SPK_FW
Contributor II
Hi,
I am using s32k344 and facing some issue to generate an interrupt every one sec.
Can you guide through the steps plz. 

If possible can you share that code base also?

Thank you
0 件の賞賛
返信

1,956件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Can you describe detail about your purpose to use RTC on S32K344 in state "my main purpose is to set and read time"
What is your input and expectation?

Does the device reset RTC domain when device is resetted or the device keeps on counting the RTC? RTC counter will reset to 0 when resetting.

cuongnguyenphu_0-1678961288387.png

 

 

0 件の賞賛
返信